Expressions.expr-primary-datetime
Use the DATE, TIME, or TIMESTAMP keywords to specify a date, time, or timestamp value.
Format
{ DATE | TIME | TIMESTAMP } { 'DateTime' | ? | ( DateTimeExpr ) }
Remarks
Follow the DATE, TIME, or TIMESTAMP keyword by the DateTime value.
The DateTime value can be one of the following:
- A string literal defining the date, time, or timestamp value.
- A parameter marker.
- A string expression enclosed in parentheses.
The resulting string is interpreted as an SQL date, time, or timestamp literal. The following table describes the required format for each type:
| Type | Format |
|---|---|
| DATE | YYYY-MM-DD |
| TIME | HH:MM:SS[.FFFFFF] |
| TIMESTAMP | YYYY-MM-DD HH:MM:SS[.FFFFFF] |
For TIME and TIMESTAMP types, the fractional seconds part [.FFFFFF] is optional.
DATE '2025-01-31'
TIME '12:55:00.000'
TIMESTAMP ('2025-01-31' || ?)
DATE ?