Expressions.expr-primary-odbc-datetime
Use the D, T, or TS keywords to specify a date, time, or timestamp value.
Format
{{ { D | T | TS } { 'DateTime' | ? | ( DateTimeExpr ) } }}
Remarks
Follow the D, T, or TS keyword by the DateTime value.
The DateTime value can be one of the following:
- A string literal defining the date, time, or timestamp value.
- A parameter marker.
- A string expression enclosed in parentheses.
The resulting string is interpreted as an SQL date, time, or timestamp literal. The following table describes the required format for each type:
| Type | Format |
|---|---|
| D | YYYY-MM-DD |
| T | HH:MM:SS[.FFFFFF] |
| TS | YYYY-MM-DD HH:MM:SS[.FFFFFF] |
For T and TS types, the fractional seconds part [.FFFFFF] is optional.
{D '2025-01-31'}
{T '12:55:00.000'}
{TS '2025-01-31 12:55:00.000'}