Query Clauses with Very Large Numbers

When creating query clauses to perform equality / inequality, operations you should consider whether large floating point numbers can be avoided as they cause rounding errors.

You should also avoid using statements similar to the following:

<Field> = "Value"

Or:

<Field> <> "Value"

Consider using < or > (less than or greater than) to select rows with large integer values as this offers a greater level of precision.

Example:

The following query clause will cause rounding errors, which makes it impractical to perform equality / inequality operations against:

( FULLSCALE <> 3.402823e+38 ) AND ( POINTTYPE < 5 )

This query would be better written:

( FULLSCALE < 100000000 ) AND ( POINTTYPE < 5 )

This gives a better result.