StringFunctions

This section describes function returning a string value.

Contents

Name Description
Character substring function Extracts a substring from the given string
Fold function Scalar functions for changing the case of text strings
Regex substring function Extracts a substring from the given string using regular epxression pattern matching
Replace function Replaces all occurrences of string_exp2 in string_exp1 with string_exp3
Soundex function Returns the Soundex code for a string expression
Translate function Returns the application dictionary translation for a string expression in the current user locale
Trim function Removes whitespace from a string