Animation Properties for Mimic Items on Layers

When using the Mimic.Layers property, you can access any of the animation properties for any Mimic item on that Layer. The properties are the same as the properties that are shown on the Animations window for that item. For example, a Remote Image item has Alignment, PickComment, PickDisabled, PickParam, PickType, PosAnchor, PosMax, PosMin, PosVal, RefreshRate, TooltipText, Url, and Visible.

There are also some additional properties that you can access which are not shown on the Animations window. These include:

For more information on the properties on the Animations window, see Using the Animations Window in the Geo SCADA Expert Guide to Mimics.