ComboBox.Add

The ComboBox Control Object that is returned by the AddComboBox function has its own functions which include the Add function. The Add function adds a selectable option to the Combo Box.

Syntax

ControlObject.Add(Text)

Where ControlObject. is the name of the variable (declared in your script) that is used to store the Combo Box Control Object that is returned by the AddComboBox function.

Description

Adds a selectable option to the Combo Box.

The option you add is inserted at the bottom of the Combo Box's list. To add an option to a different location in the list, you need to use the Combo Box's Insert function (see ComboBox.Insert).

Arguments

Text {string}

The text that is shown for the option in the Combo Box.

Returns

None.

Example:

ComboBox1.Add("All Areas")

Where:

  • ComboBox1 is the name of the variable that stores the ComboBox Control Object returned by the AddComboBox function
  • "All Areas" is the name for the option being added.