Define the Client Specific Settings for the Guest User

You can use the Options window to define whether the Guest user can access specific features from the client PC. The settings you put in place only apply to the client PC on which they are made and have no effect on the Guest user account when used on any other client or server.

To define the client specific settings for the Guest user account, display the Options window.

On the General tab, use the Guest User section to configure the local Guest User settings for this particular client:

Features

Select the Edit button next to Features to display the Features window.

Use the Features window to define which features are available to the Guest User. The settings on the Features window work in the same way as the corresponding settings on the User Form except that they apply to the Guest user account and so can be used by anybody that has access to the client.

The groups of feature settings are:

Select the OK button to confirm your choices and close the window, or select Cancel to discard your selections and close the window.

Homepage

On the Options window, use the Homepage setting to select the Homepage display for the Guest User. This works in the same way as the Homepage setting on the User Form except that it only applies to the Guest user account on this client (see Define the Home Page Settings for a User).

Locale, Date Format, Display Times in UTC

Use the Locale, Date Format, and Display Times in UTC settings to define the regional settings for the Guest User on this client only. These settings have to be set so that they are compatible with the Regional Settings on the Root Group Form (see Define the Global Settings for the Guest User Account).

Confirm Actions

Use the Confirm Actions setting to define whether the Guest user has to confirm methods before they are performed by the system. This setting works in the same way as the Confirm Actions setting on the User Form (see Enable or Disable the Confirm Actions Feature for a User).

Inactivity Shutdown

This allows you to define the period of inactivity in minutes after which ViewX is shutdown if only the Guest user is logged on. The inactivity is determined by any mouse or keyboard interaction with the user interface. The inactivity timer is used by both the Inactivity Logout and Inactivity Shutdown at the same time.

The following examples illustrate how the Inactivity logout and Inactivity Shutdown settings work together.

 

The way in which the Inactivity Shutdown settings affect ViewX depends on the settings of the Inactivity logout and the Logout on inactivity:

When the Guest user is given permissions to edit documents and they leave an unsaved changed document open in ViewX, this will prevent the automatic shutdown from triggering to prevent the loss of the unsaved work.

NOTICE

SECURITY THREAT

If the Guest User Account is configured with inappropriate permissions the security of the system may be compromised.
Failure to follow these instructions can result in a breach in the system security and loss of data.

Select the OK button to confirm your choices and close the Options window.

When you have configured the Guest user account, you will need to define its access permissions. For more information, see Allocating Security Permissions.