Exclusive Control

The Exclusive Control permission defines whether the user or User Group can take exclusive control of an item. When an item is under exclusive control, some of the features for the item are only available to the user with exclusive control.

Please refer to Exclusive Control for more information.

Availability: Can be restricted via the Permission Restrictions settings (see Define Whether any Permissions are Restricted).