Create or Modify an Extra Field

You can use ViewX on a server to create extra fields in the database. These fields are shown as combo boxes, data entry fields, or check boxes on Forms.

If you want to add an extra point data field, see Data Fields.

For more information on how to add or modify an Extra Field, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.