Define the ICMP Monitor Settings for a Server

Each Geo SCADA Expert server in a multi-server architecture performs checks on the other servers in the architecture. By default, each server performs two checks:

These default checks are used by Geo SCADA Expert to detect problems with the servers and the network connection between the servers. However, you can also configure Geo SCADA Expert to perform up to three additional ICMP checks on ICMP compatible devices that are connected to the network, such as client PCs, printers and routers. These extra checks are useful as they can also be used to provide confirmation of a network failure.

The diagram below shows a server on one side of a WAN (Site A) monitoring the server on the other side (Site B).

The server at Site B also performs the same checks on the server at Site A.

To configure the additional ICMP Monitor checks for a server:

  1. Access the System Configuration>Partners settings on the Server Configuration Tool.
  2. In the ICMP Monitor 1, ICMP Monitor 2 and ICMP Monitor 3 fields, enter the IP Addresses of the devices that are to be tested by the additional ICMP Monitor checks. For example, if you are configuring a server to perform an additional ICMP monitor check on a client and a router, you would enter the IP address of the client in the ICMP Monitor 1 field and the IP address of the router in the ICMP Monitor 2 field.
  3. If the server has a back up connection (uses dual ethernet connections), enter the IP addresses for the devices in the corresponding ICMP Monitor fields in the Backup Connection section.
  4. Right-click on the system icon in the hierarchy on the Server Configuration Tool, and then select the Apply Changes option. The ICMP settings you have made are now in place.

During normal conditions, the servers will run the TCP/IP server-server and ICMP checks continuously and return ‘healthy’ results.

If the TCP/IP check returns a ‘failed’ result, the servers use the ICMP checks to determine the reason for the TCP/IP failure: