Define the Settings for COM Ports and TCP/IP Connections

The COM port and TCP/IP connection settings define how Geo SCADA Expert reacts to a driver being unable to assign to a COM port or TCP/IP socket. They also define the number of conditions that can cause a channel (that is associated with a port/socket) to be deemed as failed.

When Geo SCADA Expert detects that a channel has failed, it raises an alarm (if configured to do so) and the channel de-assigns from the port or socket. After the specified time period, the driver attempts to re-assign the port or socket.

The default COM ports and TCP/IP Connections settings are usually appropriate, but you may need to change the settings if:

For more information on changing the COM port and TCP/IP settings, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.