Send Buffer Size

The Advanced section of the Geo SCADA Expert Server Configuration Tool's Global Parameters contains a Send Buffer setting.

The Send Buffer size defines the amount of data that is sent and received within each network write operation.

The default Send Buffer size of 8192 bytes is suitable for many systems. However, if there are network problems, the buffer size may need to be changed.

If you need to change the Send Buffer size, you will need to access the Advanced section of the Global Parameters branch on the Geo SCADA Expert Server Configuration Tool. However, do not change the Send Buffer size unless specifically instructed to do so by Schneider Electric staff.

ATTENTION: Do not attempt to change the Send Buffer size without first consulting
Schneider Electric engineers. Changing the Send Buffer size without expert advice could result in inaccurate system operation.