Uninstalling Windows Performance Monitor Counters

If you no longer want to use the performance counters you should uninstall them.

To uninstall the Geo SCADA Expert counters, use the counter tool provided within Windows as follows:

  1. Open a Command Prompt window in Microsoft Windows®.
  2. Use the cd command to change the directory to that in which the Geo SCADA Expert Performance Monitor Counter file is installed. The Tool is installed in the same directory as other Geo SCADA Expert installation files. The default location of these files varies depending on the Windows operating system (see File Locations (Default) in the Geo SCADA Expert Installation Guide).

    Example:

    If Geo SCADA Expert is installed at the default location on a machine that is running Windows 10, you would enter:

    cd c:\program files\Schneider Electric\ClearSCADA

  3. Press the Enter key.
  4. Use the dir command to check that the Geo SCADA Expertcounter file (DBKernal.man) is present.

  5. Uninstall the performance counters by entering the following at the command prompt:

    unlodctr /M:DBKernel.man