Modules

The General branch of the Server Status Tool includes a Modules category. The category provides diagnostic information about each driver that is installed on your system.

The status information is categorized as:

  • Driver—The name of the driver, for example, DNP3.
  • Publisher—The name of the company that produces the driver.
  • Version—The version number, build number, and revision number of your Geo SCADA Expert drivers. Schneider Electric engineers may ask for this information in the unlikely event that you experience unexpected behavior relating to drivers.
  • Status—The current status of the driver. This can be:
    • Running—The driver software is currently in operation.
    • Starting—The driver is starting to run. If the status is consistently Starting, the driver software is not present—contact Schneider Electric for advice.
    • Starting, Stop Pending—The driver is in the process of starting and there is a stop request pending. The starting mechanism cannot be interrupted, and so the driver will only be stopped after it has completed starting.
    • Stopping, Start Pending—The driver is in the process of stopping and there is a start request pending. The stopping mechanism cannot be interrupted, and so the driver will only be started after it stopped.
    • Stopping—The driver is attempting to stop.
    • Stopped—The driver is no longer running.
    • Stopped, No Config—The driver is not running due to there being no database items defined for that driver.
    • Invalid—Geo SCADA Expert has detected an internal driver management problem. If this status is shown, contact Schneider Electric for assistance.
    • Failed, Retry Pending—The latest attempt to run the driver software was unsuccessful. An attempt to start the driver software is due.

      With some drivers, you might need to install and reference another application in order for the driver to run. If this applies, the relevant driver guide will explain the requirements. If you have fulfilled the requirements and this state persists, please report the issue to Schneider Electric.

      If this state occurs for a driver that is correctly licensed and does not require additional software to be installed, please report the issue to Schneider Electric.

    • No License—Your system does not have a valid license for the driver.

      With an advanced driver for which one or more extension drivers are installed, the 'parent' driver might appear to be unlicensed if any of those extension drivers are unlicensed. (You can check which drivers and extension drivers are licensed by looking at the entries in the Drivers section of the License Details window on the server (see Display the License Details Window on a Geo SCADA Expert Server).) You might upgrade or otherwise change your installation of Geo SCADA Expert to include an extension driver that you want to use. To accommodate such a change, you might need to upgrade your Geo SCADA Expert license to include that extension driver. For more information, see Upgrade a License.

      If your system uses Crystal Reports, the Crystal Reports module is likely to be unlicensed on any Permanent Standby servers on your system. This is to be expected due to the lack of a Crystal Reports runtime license. The Crystal Reports prerequisites and driver need to be installed on the Permanent Standby servers in order for the database to synchronize. However, as the Permanent Standby servers do not require the Crystal Reports driver to be operational, they do not require a Crystal Reports runtime license. On all other Geo SCADA Expert servers, the Crystal Reports driver and runtime components must be licensed.

      The Crystal Reports driver is the only driver that may appear with a 'No License' state on Permanent Standby servers. This is purely due to the lack of requirement for a Crystal Reports runtime license on those servers. All other drivers must have a valid license for each server on which they are installed, including Permanent Standby servers. (To use a particular driver in Geo SCADA Expert, that driver needs to be installed on all of the servers on the system, including Permanent Standby servers, in order for the database to synchronize.)

    • No License (Can’t Demo)—Your system does not have a license for the driver and so the driver cannot be demonstrated.
    • Invalid Registration—Geo SCADA Expert cannot find the .dll file for the driver or the .dll file is inaccessible or corrupt. Typically, this only occurs if the registry settings for the driver have been incorrectly changed (manually), or if a user deletes or renames some of the Geo SCADA Expert components in the installation location.
  • Startup—The type of startup for the driver. If it is Automatic, the system starts the driver software whenever you start the server. If the Startup is Manual, you need to start the driver by using the Start or Restart features (see Start and Stop a Driver). A Startup status of Always means that the driver cannot be started or stopped.
  • Failure Count—The total number of times that the driver software has failed.
  • Objects—The number of database items that have been created for each driver. If the number is 0, the driver will not start automatically (even if the driver is set to start automatically). This is to help ensure system resources are only used by drivers that you need to run on your system.
  • For more information on starting and stopping a driver, see Start and Stop a Driver.
  • Logging Options—The logging options vary according to the driver. They correspond with the entries on the Current Options section of the Logging window (see Logging and Monitoring).

For many drivers, you can access a context-sensitive menu by right-clicking on the driver in the list.

The options that are available vary depending on the driver, but can include: