Enable Broker
Associated with: Sparkplug Publisher Broker items
Security permission required to access this pick action: Disable Points
Use this pick action to place a Sparkplug Publisher Broker database item In Service. Triggering the action changes the Broker's configuration so that its In Service property is enabled and the Broker becomes active.
The Enable Broker pick action is only available for a Sparkplug Publisher Broker:
- That is not In Service
- For which your User Account is allocated the Disable Points security permission.
unexpected impact on system performance
- The configuration of the downloaded or cloud-based broker that is represented by the Geo SCADA Expert Broker item
- The configuration of the publishing devices that are connected to that broker.
Both mentions of configuration above refer to configuration outside of the Geo SCADA Expert database.
Also see Disable Broker.
If using this pick action with the Automation Interface, you need to specify the method name Enable.