Define the Point Scaling

Use the fields in the Scaling section of the TBox Analog Input Point or TBox Analog Output Point Form to specify the type and range of the raw input signals, so that they can be suitably converted into floating-point engineering values for use in the Geo SCADA Expert database.

The scaling is also used on the TBox Analog Output Point to perform a similar conversion on any output signals. Geo SCADA Expert uses the conversion calculation to produce a raw data value that is sent to plant.

There are two levels of scaling that can be applied to a TBox Analog Point. The first level is scaling a raw value into an engineering value using linear interpolation. This level of scaling is applied only if the RTU returns an integer value. At this level, if the RTU reports the value as a floating point value, Geo SCADA Expert ignores any configuration in the Raw Full Scale and Raw Zero Scale fields, regardless of the Enabled setting. The second level of scaling is where the Multiplier and the Offset values are applied. This second level of scaling is always applied.