Scanner Configuration Fields

A Totalflow Scanner item has additional configuration fields that do not appear on the configuration form, which are listed in the Geo SCADA Expert Database Schema.

  • Logging Level— This field controls the level of detail in the driver module’s log file for actions related to this scanner. A value of 0 means that the log file contains errors only and a value of 4 means that the log file is extremely verbose. For more information on logging, see Driver Log File.