Configure a Y-Axis

You can change the configuration of any of the Y-Axes that are shown on a Trend (provided your User account has the Configure permission for the Trend).

To configure a Y-Axis:

  1. Display the Trend that has the Y-Axis that you want to change (see Display a Trend in Design Mode).
  2. Right-click on the Y-Axis that you wish to configure.
    A context sensitive menu is displayed.
  3. Select the Edit... option.
    The Edit Y-Axis Window is displayed.

    Edit Y Axis

  4. Use the Edit Y Axis window to change the settings for the Y-Axis. The settings on the Edit Y-Axis window work in the same way as the settings on the Add Y-Axis window (see Add a Y-Axis).

    This means you can configure the:

    • Name of the Y-Axis
    • Position of the Y-Axis on the Trend
    • Label of the Y-Axis
    • Scaling of the Y-Axis
    • Ticks on the Y-Axis.
  5. Select the OK button to confirm your choices and close the Edit Y-Axis window.
    Your Trend will display with the settings you selected.
  6. Save the configuration.