Trend Key

The Key is displayed at the bottom of the Trend display. It lists the traces that are shown on the Trend and provides information about the source of the trace (its values, category, and so on).

Trend Key

Each row of the Key provides information for one of the traces on the Trend. By default, the key displays information in four columns: Trace, Type, Ruler Value, and Axis. If your User account has the Configure permission for the Trend, you can use the Columns feature to display different or additional columns (see Define the Columns on the Key).

By design, the columns displayed here are evaluated from the raw historic data, whether the trace type is Raw Historic or Processed Historic (see Configure a Trace).

The predefined columns that can be displayed in the key include:

Embedded Trends on Mimics provide a subset of the features that are available on pre-configured Trends. This includes operational-level access to a subset of the menu options on the Trend. Trends that have been configured to display in Inset Windows on Mimics support a slightly different subset of operational-level menu options to Embedded Trends.