Specify Whether to Include the Stream Identifier in each Data Packet

Trio radios are capable of communicating via one of multiple message streams. Of the Trio radio series with which Geo SCADA Expert can communicate, radios other than D Series can use a Stream Identifier ( SID) code to identify the particular message stream that is being used.

Select the Send SID check box on the Channel tab if the radio port that Geo SCADA Expert uses to communicate with the ‘base’ Trio radio is one of the following:

With such communications, use the Stream ID field on each Trio Diagnostics Radio Form to specify the actual message stream used by each radio (see Specify the Stream on which the Radio is to Transmit Messages).


Clear the Send SID check box if:

or: