Created
Associated with: All items
Do not confuse this status attribute with the Created status attribute that is supported by driver-specific database items on some drivers. The driver-specific status attribute is documented in the relevant driver guides.
This status attribute is only displayed for new items. It is replaced with the Last Modified attribute as soon as an item’s configuration is modified.
The Created attribute indicates the date and time at which an item was added to the database. The attribute also lists the name of the user that was logged onto the system from that node (workstation) at the time.
Example:
2025-05-29 10:05:32 by Engineer1
(Indicating that an item was added to the database at the time and date that is specified. ‘Engineer1’ was the user that was logged onto the workstation at that time.)