Display Alarm View

This option is only available if an Alarm View is configured for the item or the Group with which the item is associated (see Define an Alarm View).

Use the Display Alarm View option to display the ‘file object’ (such as a Mimic or Trend) that is configured as the item’s Alarm View.

Use the Alarm View to ascertain further information about any alarm(s) and/or take the appropriate action. For more information about alarms, see Alarms.

With a ViewX client on a Multi-Monitor Setup, you may be able to select the name of the Window Container in which to display or edit a document. Each Window Container displays on a particular monitor by default. Such options are only available when you select certain Display... or Edit... pick actions from the Database Bar or Operator Documents Bar. For more information, see Ability to Specify the Window Container in which to Display or Edit a Document.