Remove with Comment

Associated with: Any item for which an alarm can be raised

Security permission required to access this option: Remove Alarms

WARNING

LACK OF ALARM NOTIFICATION

Use the Remove with Comment option with care. Before using the option, we strongly recommend that you perform a risk analysis to ensure that the removal of existing alarms will not pose a danger to people or equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage

Use the Remove with Comment option on the Object Menu to add a comment to the Event Journal when Geo SCADA Expert removes any acknowledged alarms from the selected item, Group or Group Instance (and any subgroups within that Group or Group Instance).

For more information, see Remove an Alarm with Comment.

If using this pick action with the Automation Interface, you need to specify the method name RemoveAlarmWithComment.