Status Bar

The Status Bar is not displayed in full screen mode. The Virtual ViewX client is always displayed in full screen mode hence the status bar is not displayed on a Virtual ViewX client.

The status bar is displayed at the bottom of The ViewX Window.

The status bar displays:

The Status Bar can also be set to display the current time. This feature can be enabled by a user whose user account provides access to the Options window (see Miscellaneous Options for ViewX clients).