Understand the 'All Windows and Layout' Functionality

You can use the 'All Windows and Layout' option to save the layout of multiple displays (such as Trends, Mimics, Reports, and/or Lists) as a collective Favorite display (see Add a ViewX Display to your Favorites List). When you view the Favorite, each of the documents that make up the Favorite are displayed in their relative positions. This topic provides further information about how different scenarios affect the documents in an 'All Windows and Layout' Favorite.