Configure the Font used for the Axis

You can change the appearance of the font that is used for the y-axis text. You do this using fields in the Y-Axis Properties window (see Configure the Y-Axis Properties).

Use the Fonts section of the window to specify the font's appearance: