Configure the Trace's Label

You can specify a label for a trace. The label is a text string that identifies the trace. You specify the label using a field in the Trace Properties window (see Configure a Trace).

Label Font

The font settings associated with a trace's label are common to all trace labels on the X-Y-Z Plot. You specify the settings using the Fonts section of the X-Axis Properties window (see Configure the Fonts used for the Axis and Trace Labels). Set the Fonts option to Trace Labels and then specify the properties of the font that you want to use for the trace labels.

Label Color

The color of the label text is common to all trace labels on the X-Y-Z Plot. You specify the color in the X-Axis Properties window (see Configure the Position of the Axis and the Color of the Axis and Trace Labels).