Configure the Y-Axis Color and Position

You can specify the color and position of the y-axis. You do this using fields in the Y-Axis Properties window (see Configure the Y-Axis Properties).

Use the Axis section of the window to specify these axis properties: