Configure the Ticks for the Axis

You can specify the number of ticks that are included on the y-axis. You do this using fields in the Y-Axis Properties window (see Configure the Y-Axis Properties).

Use the Ticks section of the window to specify these properties: