Understand X-Y-Z Plots

X-Y-Z Plots are special types of Trends that allow you to monitor the relationships between multiple sets of historic values. The configuration of each X-Y-Z Plot provides a 'three-dimensional' ('3D') graphical representation of sets of historic values, with the z-axis providing the 'depth', in the form of a time line.

Each X-Y-Z Plot consists of:

The data on an X-Y-Z Plot can be displayed in one of three drawing modes. The drawing mode determines the connection lines that Geo SCADA Expert draws between the data values on the X-Y-Z Plot:

Examples:

An X-Y-Z Plot showing data in 'Connect by Point' mode:

The same data shown in 'Connect by Timestamp' mode:

The same data shown in 'Connect by Point and Timestamp' mode: