View Information about a Particular Data Value

Information about a trace's data values is available in the form ToolTips—one ToolTip per data value.

To display the ToolTip for a particular data value, place the cursor over the relevant trace marker. (If the trace's markers are hidden, either redisplay them or move the cursor along the trace until it is over a data value—a ToolTip appears when the cursor moves over a data value.)

Each ToolTip provides the following information:

Either:

And

Example:

The ToolTip shown below is for a data marker that has a value of 75.45. Geo SCADA Expert processed the value at the date and time shown on the ToolTip. The data value's source is 'Sensor 2'. The database item that represents the sensor is stored in the database in the Group 'Zone 1' (which is itself located in the Group 'Eastern Region').