Mounting the Inverter

  WARNING

heavy equipment

  • The Inverter weighs approximately 102 lb (46.4 kg). A minimum of two people must be present to lift the inverter. To prevent personal injury, always use proper lifting techniques during installation, and follow local work safety rules.

  • Do not lift the inverter using the heatsink cover.

  • For structural and seismic stability, the Inverter must be mounted onto a vertical supporting surface strong enough to support the Inverter and all other equipment that is installed on the same surface.

  • Use mounting hardware that is appropriate for the mounting surface and weight of the Inverter.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

IMPORTANT: If you are installing a Schneider Boost battery with the inverter, the battery must be installed first.

To mount the Schneider Inverter:

  1. Install the wall mount bracket(s) as shown below. Dimensions shown are from the floor to the mounting slots. IMPORTANT:  If you are installing a Schneider Boost battery with the inverter, the battery must be installed first.

    Installing wall bracket(s)

  2. With a minimum of two people, lift the inverter up to the wall bracket.

    Lifting the inverter

  3. Tilt the inverter until the inverter's bracket is behind the wall mount bracket. Then slide the inverter down until the brackets are as shown below.

    Install inverter onto mounting bracket

  4. Remove handles from the inverter and then install a #10-24 screw to attach the bracket to the bottom of the inverter, as shown below. Torque to 5 Nm (43.7 in-lbs).

    Lifting the inverter