Manual integration steps without using the web application Integration Utility settings
This section describes how to manually integrate Building Operation and PME without using the web application Integration Utility settings. Sometimes manual steps are more convenient for certain tasks, for example: making minor changes to the system.
NOTE: The manual steps cannot fully replace the web application Integration Utility settings for an PME/EBO Integration deployment. When deploying the PME/EBO Integration, you must use the web application Integration Utility settings to create the Diagram links.
The following manual steps are described in this section:
- Creating PME users for Building Operation
- Creating Diagrams, Reports, and Dashboards links in Building Operation
- Hosting EWS values in Building Operation