Device Networks
This section provides information on the communication links between the software and the monitoring devices.
Use the links in the following table to find the content you are looking for:
Topic | Content |
---|---|
Device networks overview | Device network basics and the supported protocols and device types. |
Network types | Ethernet and serial communication networks. |
Network performance | Ways to improve the device communication performance. |
Time synchronization | Time synchronization on the monitoring device network. |
Tools | The Daisy Chain Calculator tool. |