Planning checklist
The following checklist has an entry for each of the sections in the planning chapter of this
Item | Details | Completed |
---|---|---|
System Architecture | Decide which architecture to use (Standalone, Distributed Database). | □ |
Client Types | Decide which type of clients and how many of each are needed (Web Clients, Engineering Clients). | □ |
IT requirements | Decide which computer hardware, and operating software to use (OS, SQL Server). Understand the network related dependencies, and plan for them. |
□ |
System maintenance | Understand the system maintenance needs and recommended actions. | □ |
Disaster recovery strategy | Understand on disaster recovery and recommended strategy | □ |
Licensing | Understand which licenses (PME, OS, SQL, ...) are required for your system and plan to purchase them in time for the deployment. | □ |
System installation and upgrades | Understand the prerequisites and the different options for new installs and upgrades. | □ |
Feature Selection and design | Define which features and modules you want to setup for the user. Understand the prerequisites and dependencies, and plan for them. |
□ |
Device networks | Understand the device network options (Ethernet, serial). Match the devices with features and modules (device capabilities, performance, and so on). |
□ |
Cybersecurity | Understand the security needs of your customer and application. Develop a security strategy and plan for the system, the network, the devices, and other relevant components (data encryption, virus and malware detection, firewalls, ...). | □ |
System integration |
Understand the different approaches and technologies for integrating PME with other systems, for example, OPC, EWS, ETL, ODBC, PQDIF, VIP, .... |
□ |
Deployment considerations | Understand the complexity of the deployment and the time and expertise required. | □ |