Verify install file integrity and authenticity

warning

potential compromise of System availability, integrity, and confidentiality

Use cybersecurity best practices to help prevent unauthorized access to the software.

Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.

Work with facility IT System Administrators to ensure that the system adheres to the site-specific cybersecurity policies.

Verify the file integrity and authenticity for software updates and other components before installing them in the system. Do not install files for which the integrity and authenticity cannot be confirmed.

For details on how to verify file integrity and authenticity, see Verifying file integrity and authenticity.