Configuration Manager
Because configuration information is stored in the software in various places such as the database, the Windows Registry, the file system, and configuration files, managing a PME configuration is a complex, time consuming operation.
Configuration Manager reduces the time it takes to work with PME configurations by reading and displaying a system's configuration information. Once read, you can inspect and save the configuration information to an archive file. You can then transfer the archived configuration information to other systems.
NOTE: Configuration Manager is an add-on tool for PME. It is not included in the software install.
This help file contains information to help you understand: