Generator Performance Configuration Tool with EPSS Test Module

TIP: You can open the Generator Performance Configuration Tool from the Power Monitoring Expert > Configuration Tools folder on your desktop.

Use the Generator Performance Configuration Tool to configure the Backup Power Module and the Capacity Management Module. With this tool you define Generators, Transfer Switches, Equipment, and Groups for the Generator Activity, Generator Battery Health, Generator Test EPSS, Generator Load Summary, Equipment Capacity, and Generator Capacity reports. You also use this tool to generate the EPSS Vista diagrams, and to manage the Run History of the Generators.

The report templates have different configuration requirements. Not all of the components and properties available in the configuration tool have to be configured for all of the report templates. See the Backup Power Module configuration section and the Capacity Management Module section in the System Guide for details.

Prerequisites
  • The monitoring devices that are recording the generator, transfer switch, and equipment data must be configured in the PME Management Console and must be communicating before you can configure the components and properties in the configuration tool.