Power Losses Configuration Utility
TIP: You can open the Power Losses Configuration Utility from the Power Monitoring Expert > Configuration Tools folder on your desktop.
Use the Power Losses Configuration Tool to configure the Capacity Management Module. With this tool you define Transformers and UPS Modules for the Power Losses Report.
Prerequisites
- The monitoring devices that are recording the transformer and UPS data must be configured in the PME Management Console and must be communicating before you can configure the components and properties in the configuration tool.
User Interface
Control | Description |
---|---|
Help | Opens the help for the utility. |
New | Creates a new entry in the grid. |
Delete | Deletes the selected entry from the grid. |
OK | Saves all changes and exits the utility. |
Cancel | Exits the utility without saving changes. |
Apply | Saves all changes and leaves the utility open. |
Grid Area Columns | Description |
---|---|
Modified | Displays a status symbol for the record. |
+ (plus) | A new entry. |
* (asterisk) | An existing entry has been modified. |
! (exclamation mark) | The entry is incorrect. |