Meter apportionment
Meter apportionment allows you to assign a percentage of a device that has been assigned to an area. For example, if a common area is monitored by a single meter but shared by two tenants, for billing purposes you might want to allocate only a portion of the meter to each tenant. If tenant 1 uses 60% of the common area and tenant 2 uses 40%, you can attach 60% of a meter's reading to the tenant 1 area node and the other 40% to the tenant 2 area node.
See Creating an apportioned meter for more information.