Log Viewer

TIP: You can open Log Viewer from the SETTINGS > System > System Log page in Web Applications.

Use Log Viewer to view PME system events. System events are logged by the software and its components to record certain system activities. Examples of system events include a user logging on, a user logging off, time synchronization sent from the system to the devices, system warnings, and so on.

NOTE: The Log Viewer only shows system events, it does not show device based events or historical data. To view device event log data, use Alarm Views. To view device historical data, use Dashboards, Diagrams, or Reports.

Log Viewer User Interface

1

Date Range Selector.
Select the time range for which you want to display the system log entries.

2

Max Records.
Set the maximum number of entries to be displayed in the system log table.

3

Minimum Priority.
Filter lower priority log entries from the system log table view.
The available options, in increasing priority order, are: Diagnostics, Information, Warning, Error, Critical.

4 Log Type.

Filter log entries in the system log table view based on the area of the software where they originated.
The available options are: All, Application (= web application components), System (= platform components).

5 Category Filter.

Filter log entries in the system log table view based on the component or function they relate to.
The large number of different category options is available for this filter.

TIP: Selecting the Audit category shows user login and logoff activity.

6 Location Filter.
Enter a filter string into the text box to filter the system log table view based on the Location column information.
7 Message Filter.
Enter a filter string into the text box to filter the system log table view based on the Message column information.
8 Details Filter.
Enter a filter string into the text box to filter the system log table view based on the Details column information.
9 Column Selector.
Select which columns are displayed in the system log table.
10

Refresh.
Reload the content of the system log table.

11

Copy Selection to Clipboard.
Copy the content of selected system log table entries to the clipboard, for use in another application. Information for all possible columns is included in the copied details, regardless if the columns are displayed in the table view or not.

TIP: Use Shift + click or Ctrl + click to select multiple rows in the table.

12 Export

Export the content of selected system log table entries in .csv file format, for use in another application. Information for all possible columns is included in the copied details, regardless if the columns are displayed in the table view or not.

TIP: Use Shift + click or Ctrl + click to select multiple rows in the table.

13

Search Logs

Enter a filter string into the text box to filter the system log table view based on the Details column information.

14

System log table
The System log table shows system events for the selected time range and filter settings. See 1-8 above.

TIP: Double-click a row in the table or select a row and hit Enter to view details for this log entry.

15

Number of displayed items
Shows the number of items visible on this page, and the total number for the selected time range and filter settings. See 1-8 above.

16 Page selector.
Use the page selector to navigate between pages. Set the number of items that are displayed on a page.