Trends configuration
warning
inaccurate data results
● | Do not incorrectly configure the software or the devices. |
● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
● | Consider the implications of unanticipated transmission delays or failures of communications links. |
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
warning
unintended equipment operation
● | Do not use the software to control time-critical functions. |
● | Do not use the software to control remote equipment without proper access control and status feedback. |
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Open the Trends application from the TRENDS link in the Web Applications banner.
For information on how to configure the Trends application, see:
For reference information see:
For information on how to use Trends, see Trends.