Database Manager
Use Database Manager to manually perform operations on the Power Monitoring Expert databases.
notice
LOSS of data
● | Back up the database at regular intervals. |
● | Back up the database before upgrading or migrating the system. |
● | Back up the database before trimming it. |
● | Back up the database before making manual database edits. |
● | Verify correct database behavior after making database or system changes. |
Failure to follow these instructions can result in permanent loss of data.
NOTE: Database Manager does not include manual database operations on the Application Modules database (ApplicationModules). In a disaster recovery situation or when directed by Technical Support, the Application Modules database can be restored by using the Restore database function in the SQL Server Management Studio. See Restoring a database for further information about this operation.
For information on database maintenance tasks in PME, see Database maintenance.