Supported measurements and devices

The following measurements have been pre-mapped in the Sample WAGES rate file:

Power
Measurement Unit ION Name
Block Demand Apparent Power Total kVA Apparent Power Sliding Window Demand Delivered+Received
Block Demand Reactive Power kvar Reactive Power Sliding Window Demand Delivered - Received
Block Demand Active Power kW Active Power Sliding Window Demand Delivered-Received
Energy
Measurement Unit ION Name
Apparent Energy Total kVAh Apparent Energy Delivered + Received
Reactive Energy Into the Load kvarh Reactive Energy Delivered
Active Energy Into the Load kWh Active Energy Delivered

The Energy by IT Customer Report supports the measurements listed in the tables below. Only one measurement of each type (Energy , Current) is required. If multiple types of the same measurement exist in the system, then a look-up method is used to determine which one to use. The tables list the supported types in order of look-up priority.

NOTE: You can edit this list of measurements in the PME database.

Energy
Measurement Unit ION Name ION Label
Active Energy kWh Active Energy Delivered – Received kWh del-rec
Active Energy Into the Load kWh Active Energy Delivered Active Energy Delivered
Current
Measurement Unit ION Name ION Label
Current Average Mean A Current Phase Average Mean I avg mean
Block Demand Current Avg Into the Load A Current Phase Average Sliding Window Demand Delivered Amps Avg Dmd
Current Avg A Current Phase Average Current Avg

The following devices can provide the measurements required for this report:

  • BCPM-E, PM5350 (multi-circuit mode)
  • Basic, Intermediate, or Advanced Device for main service entrance (PM5xxx, PM8xxx, ION7650, ION9000)