Supported devices
The Breaker Performance reports automatically read the required measurements from the breaker control units. No measurement selection or configuration is required. Not all control unit types support all the measurements shown in the report. Unsupported measurement data is shown as "N/A" in the report.
The Breaker Aging Report and Vista diagrams supports the following device types:
Standard / Country | Circuit Breaker Range | Control Unit Range |
---|---|---|
IEC |
|
|
China |
|
|
USA |
|
|
The Breaker Settings Report supports the following device types:
- Micrologic 2 A/E/X/Xi
- Micrologic 3 A/X/Xi
- Micrologic 5 A/E/P/H/X/Xi
- Micrologic 6 A/E/P/H/X/Xi
- Micrologic 7 A/P/H/X/Xi
- Micrologic 5.2 A/E (Compact NSX)
- Micrologic 6.2 A/E/E-M (Compact NSX)
- Micrologic 5.3 A/E (Compact NSX)
- Micrologic 6.3 A/E/E-M (Compact NSX)
- Micrologic 7.2 A/E (Compact NSX)
- Micrologic 7.3 A/E (Compact NSX)
NOTE: The IFE/IFM versions of the above device types are supported as well.