Notification delay example
The following example shows how the delay settings for notifications affect the message delivery.
Example settings:
Initial Delay (seconds) = 10
Incremental Delay (seconds) = 7
Maximum Delay (seconds) = 30
A - New alarm activity occurs every 5 seconds
B - Initial and incremental time delays
C - Notification message is sent after maximum delay of 30 seconds
NOTE: After the maximum delay, a notification message is sent that includes all alarms that were active in the notification time window up to the maximum delay cut off. In the example above, 6 alarms would be included.