Reports UI

1 Report Library
The Report Library contains all the Reports that are configured in the system. Reports can be listed individually, or they can be organized within folders.

TIP: To hide the library, click the Hide Library icon ( or ) in the top right corner of the library. To show the library, click the Show Library icon ( or ) at the top of the library ribbon, or click anywhere in the minimized library ribbon.

2 Reports Inputs panel
The top part of the Reports Display pane shows the inputs for the selected report. Different reports have different input types. Some inputs are preset with default values, others are unassigned and must be set before the report can be generated.
3

Hide Report Inputs / Show Report Inputs link
Click this link to hide or show the report input panel.

4

Generate Report button
Click this button to generate the report after you have set all the required input parameters.

5

Report Display panel
View the report output after generating the report. Use Download report as, at the top of the panel, to download the report in PDF, Excel, or Tiff image format.