Schedules Configuration UI
1 | Schedule Name
Provide a name for the schedule. |
2 |
Schedule Preview
|
3 | Schedule Configuration
Add rows to define the Start Times, End Times, and days of the week when the schedule is active. Define if the schedule enables or disables the function that is controlled by it. |