Replace the Config Folder

  1. Stop all ION Services:
    1. In Control Panel\Administrator Tools\Services, stop the ION Network Router service. This stops all ION services.
    2. Stop the ApplicationModules CoreServicesHost service. This stops all ApplicationsModules services.
  2. Copy the backed up \config folder to the C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert folder. This will update the \config folder with all the files that were unique to the original installation.
  3. Leave the ION and ApplicationsModules services stopped to restore a database (Restoring the Databases from the Old System).