Configure
This section describes the different tools and tasks for configuring Power Operation.
Use the links in the following table to find the content you are looking for:
| Section | Description |
|---|---|
| Configuration prerequisites | Things to consider to help you prepare for configuring a Power Operation project. |
| Changing configuration on a running system | Describes configuration changes that can be made on a running system. |
| Configuration tools | An introduction to the Power Operation configuration tools. |
| SCADA Projects | Creating a Power Operation project using Project Setup, and compiling, backing up, an restoring a project. |
| Devices |
Information and tasks on how to configure and work with:
|
| Power Operation Runtime |
How to configure and work with:
|
| Web Applications |
How to configure and work with:
|
| Applications | Information on extending the capabilities of Power Operation by configuring applications. |
| Managing user accounts, roles, and mapping | Configure and manage user access. |
| Customize default behaviors | How to use Cicode to customize a project, localizing a project, and running PO as a Windows Service. |
| System Startup and Validation Checks | How to validate your configured system on startup. |
| Distributed systems |
How to configure:
|
| Redundant systems | How to configure a redundant server. |
For more detailed resources on configuration, see the Configure references section.